User Activity

Posted on October 07, 2015 at 08:31hi !    there is a hard to knowing about scand mode with ADC  for me  i using hal library  set up it by CubeMX  there is real  code  send at  link below http://codepad.org/wKi5gSEGso   - at line 142 delare attribul...
Posted on August 26, 2015 at 11:54 hi !! i like as the question  , i   can see the Hal_GetTick() will return the variable uWick that is uni32_t type  and increment one unit when the systick interrupt happen .and  will it overflow when the uint32 typ...
Posted on August 17, 2015 at 06:42 hi my friends ,   the HAL  library is new for me and i can't to use it  effect like as the old . so  , i can use the CubeMX  to generate without HAL thanks and best regards 
Posted on August 12, 2015 at 19:30hi!!!  when  using stm32f3 discovery board normally ,  the sudden  error has occurred  ,so , i send some of  picture link  about my error https://screencloud.net/v/WFYhttps://screencloud.net/v/whau  if u have experi...
Posted on August 05, 2015 at 18:49hi my friend !!! like as the tittle ,  i looking for a funny time with stm arm7 and the kinect camera , i think it incredibly useful for robot toy application thanks and best regards