cancel
Showing results for 
Search instead for 
Did you mean: 

I can't get spi communication.

baby_chicken
Associate III

Hello.


I tried to use an imu that was previously working using the spi2 port of the stm32f4 series with the spi4 port of the stm32h7 series, but I cannot communicate with it. (imu is using icm42688p.)
Is it possible that I have made a mistake in my settings or something?

↓Configuration in the stm32f4 series.

スクリーンショット 2024-11-11 190140.png

 

↓Configuration in the stm32h7 series.

スクリーンショット 2024-11-19 201830.png

baby_chicken_0-1732015139757.png

 

Best regards.

 

3 REPLIES 3
Pavel A.
Evangelist III

IMUs are complex devices, usually they have non-volatile configuration and so on. The problem can be on the IMU side.

 

So you're saying that the settings are fine and I should try with a different imu?

baby_chicken
Associate III

I would like to know if there is some code or other that would turn on spi programmatically.