2024-09-01 06:34 AM
Default Image Configuation setting is :
Framework Features:
Size of .bin file
Touch Gfx setting in IOC file:
I also followed the link:
But still size is 2.13 GB.
Can you please help me to reduce the size of binary?
2024-09-01 08:09 AM
Don't use a .BIN to describe two regions with large separation within the ARM's 4GB address space.
Use a .HEX, or divide into two or more .BINs describing the 0x08000000 and 0x90000000 regions separately.
2024-09-01 08:14 AM
In project settings uncheck bin file create.... you have hex ok.