cancel
Showing results for 
Search instead for 
Did you mean: 

I am new to MCU programming. I'd like to test SPI loopback using HAL. The project was generated by CubeMX for STM32F411RE. The SPI_call() is called inside the main. I am unable to receive the characters in the terminal.

PRaja.1
Associate
void SPI_call()
{
	char msg[] = "smile";
	char copy[6];
	HAL_SPI_Receive_IT(&hspi1, (uint8_t *)copy, strlen(copy));
	HAL_SPI_Transmit(&hspi1, (uint8_t *)msg, strlen(msg), 100);
}
 
static void MX_SPI1_Init(void)
{
 
  /* USER CODE BEGIN SPI1_Init 0 */
 
  /* USER CODE END SPI1_Init 0 */
 
  /* USER CODE BEGIN SPI1_Init 1 */
 
  /* USER CODE END SPI1_Init 1 */
  /* SPI1 parameter configuration*/
  hspi1.Instance = SPI1;
  hspi1.Init.Mode = SPI_MODE_MASTER;
  hspi1.Init.Direction = SPI_DIRECTION_2LINES;
  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
  hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
  hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
  hspi1.Init.NSS = SPI_NSS_SOFT;
  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
  hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
  hspi1.Init.CRCPolynomial = 10;
  if (HAL_SPI_Init(&hspi1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN SPI1_Init 2 */
 
  /* USER CODE END SPI1_Init 2 */
 
}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0