2025-07-16 2:29 AM - last edited on 2025-09-01 7:20 AM by Andrew Neil
2025-09-01 7:14 AM - edited 2025-09-01 7:31 AM
Hello @NiM ;
First of all, I apologize for my late reply.
The design is not sensitive to these parameters (tr and tf).
In bypass mode the signal goes through a GPIO input. So for STM32H7 the constrains are the same as for a GPIO input.
You should respect the VIL and VIH threshold provided in table "Table 60. I/O static characteristics"
I hope this answer your request.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-01 7:28 AM
THSE is just the period of the signal; ie, 1/fHSE_ext
2025-09-01 7:31 AM - edited 2025-09-01 9:28 AM
@KDJEM.1 wrote:The design is not sensitive to these parameters.
So why does the datasheet call them out like this?
I think the datasheet needs an update to either remove them, or to say that they're unimportant.