cancel
Showing results for 
Search instead for 
Did you mean: 

hs usb stm32f429zi

John Doe1
Associate III
Posted on March 01, 2017 at 15:17

Hi,

Does stm32f429zi support usb in hs mode? i found that PB 14 is required by USB-HS but on that pin red led is connected.

Thanks for support.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Khouloud GARSI
ST Employee
Posted on March 02, 2017 at 15:42

Hi

Doe.Joe

‌,

  • In deed, the STM32F429ZI supports the USB HS mode. The OTG_HS interface supports anULPI interface for external HS PHY ; The ULPI interface needs PB13 as ''OTG_HS_ULPI_D6'';

  • I think you are using an STM32 Nucleo On this board:

    • A red user LED is connected to PB
    • If jumper JP7 is present, the PB13 pin is connected to Ethernet PHY as ''RMII_TXD1''.

Since you need this pin for USB HS transfers,please follow the steps below:

1. Configure the PB13 as ''Reset State''.

0690X00000606TSQAY.png

2. Configure the External Phy depending on your needs (OTG/Dual_Role_Device, Host_Only, Device_Only).

0690X00000606TTQAY.png

You will notice that the CubeMX tool has configured all the pins needed by the ULPI interface.

Khouloud.

View solution in original post

3 REPLIES 3
Khouloud GARSI
ST Employee
Posted on March 02, 2017 at 15:42

Hi

Doe.Joe

‌,

  • In deed, the STM32F429ZI supports the USB HS mode. The OTG_HS interface supports anULPI interface for external HS PHY ; The ULPI interface needs PB13 as ''OTG_HS_ULPI_D6'';

  • I think you are using an STM32 Nucleo On this board:

    • A red user LED is connected to PB
    • If jumper JP7 is present, the PB13 pin is connected to Ethernet PHY as ''RMII_TXD1''.

Since you need this pin for USB HS transfers,please follow the steps below:

1. Configure the PB13 as ''Reset State''.

0690X00000606TSQAY.png

2. Configure the External Phy depending on your needs (OTG/Dual_Role_Device, Host_Only, Device_Only).

0690X00000606TTQAY.png

You will notice that the CubeMX tool has configured all the pins needed by the ULPI interface.

Khouloud.

Posted on March 02, 2017 at 17:26

Thank you

garsi.khouloud

‌ !

Posted on March 03, 2017 at 10:38

You are welcome

If you have further questions, do not hesitate to post them in our forum.

Khouloud.