2025-06-07 11:41 AM
Hi, I assume there have already been posts on this topic, but I can't handle this problem. I have an STM32F429I-DISC1 board and I'm trying to connect it as a USB HID keyboard. Unfortunately, all the guides and articles don't work, and my board isn't even detected by the computer after uploading the program. Why? Has anyone else had this problem and would like to share a solution?
2025-06-07 12:58 PM
Start a CubeMX project on this board from the Board Selector.
Change USB host to USB device and add HID usb device in middleware.
Generate code.
Compile.
Run code.
Works here.
2025-06-07 2:05 PM
Could you please create a project and send it to me? I made the project as you suggested but I have already tried these settings but I still have a problem with the connection. My computer and others I have checked do not detect this board as a USB or keyboard or mouse. Thanks in advance for your help.
2025-06-09 1:55 AM
Hello @Husteczka
You can refer to this knowledge base article that explains how to implement a USB HID keyboard device from a USB HID mouse application
BR Gyessine
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.