2021-04-19 6:51 AM
i wish to use HRTIM as general purpose timer with high resolution.
can i get sample code for HRTIM .
Solved! Go to Solution.
2021-04-19 8:06 AM
You will find sample code in the repositories for STM32, e.g. on Github in some examples for NUCLEO-G474RE.
When your question is answered, please mark this topic as Answered by choosing Select as Best. This will help other users find that answer faster.
Good luck!
/Peter
2021-04-19 8:06 AM
You will find sample code in the repositories for STM32, e.g. on Github in some examples for NUCLEO-G474RE.
When your question is answered, please mark this topic as Answered by choosing Select as Best. This will help other users find that answer faster.
Good luck!
/Peter
2021-05-02 3:15 AM
i want to use HRTIM for general purpose timer with high resolution.
i dont fid the examples for time like, start and stop and get-time
2021-05-03 12:38 AM
Please take a look at the AN4539 - HRTIM cookbook.
Regards
/Peter
2021-05-10 10:22 PM
Hi Anand,
I use all 12 HRTIMs channels in my NUCLEO-G474RE port of MIcroPython.
https://forum.micropython.org/viewtopic.php?f=3&t=9082
This is a high resolution PWM application where I use a custom modg4ex.c to add HRTIM support. You can get a lot of mileage with the STM32CubeMX app to generate the initial 'C' code. The CubeMX generates brute force inline code for each channel so you need to refactor it into subroutines to shorten it up. The G474 is still a new beast so the cookbook and examples are of limited help.
best regards, RealSparky from the micropython forum