cancel
Showing results for 
Search instead for 
Did you mean: 

HRTIM 100% duty cycle

DSchm.3
Associate II

Hello,
is there a solution to generate duty cycles between 0...100% with the HRTIM? I tried up-counting mode and center-aligned mode, but I wasn't able to achieve it. 

Regards
Dominik Schmid

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

HRTIM has a few limitations, e.g. it cannot generate PWM at real 0% or 100%, as can also be found in RM0440:

  • The minimum value must be greater than or equal to 3 periods of the fHRTIM clock. The value 0x0000 can be written in CMP1 and CMP3 registers only, to skip a PWM pulse. See Section: Null duty cycle exception case for details
  • The maximum value must be less than or equal to 0xFFFF - 1 periods of the fHRTIM clock.

The second point concerns the requested 100%, which is always at least one HRTIM period smaller. And section Null duty cycle exception case says:

The high-resolution behavior is not supported for pulses narrower than 3 tHRTIM periods [...] and any value strictly below 3 periods of the fHRTIM clock [...] in the HRTIM_TIMxCMPy register is forbidden[...]. However, it is possible to skip an output pulse and have a null duty cycle by simply writing a null value in the following two registers: HRTIM_TIMxCMP1 and HRTIM_TIMxCMP3, if and only if the following conditions are met: [...]

For any other use case, this can be done by programming the SET and RESET events with the very same compare values, above 3 periods of the fHRTIM clock.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

HRTIM has a few limitations, e.g. it cannot generate PWM at real 0% or 100%, as can also be found in RM0440:

  • The minimum value must be greater than or equal to 3 periods of the fHRTIM clock. The value 0x0000 can be written in CMP1 and CMP3 registers only, to skip a PWM pulse. See Section: Null duty cycle exception case for details
  • The maximum value must be less than or equal to 0xFFFF - 1 periods of the fHRTIM clock.

The second point concerns the requested 100%, which is always at least one HRTIM period smaller. And section Null duty cycle exception case says:

The high-resolution behavior is not supported for pulses narrower than 3 tHRTIM periods [...] and any value strictly below 3 periods of the fHRTIM clock [...] in the HRTIM_TIMxCMPy register is forbidden[...]. However, it is possible to skip an output pulse and have a null duty cycle by simply writing a null value in the following two registers: HRTIM_TIMxCMP1 and HRTIM_TIMxCMP3, if and only if the following conditions are met: [...]

For any other use case, this can be done by programming the SET and RESET events with the very same compare values, above 3 periods of the fHRTIM clock.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.