2017-04-21 2:33 PM
Hi
I use STM32f779 and i have TFT LCD 800x480 controller tft is
RA8875 . I want to transfert my images to flash after i need to transfert to SDRAM and transfert to controller RA8875 . Can you help me how transfer the images to flash (QSPI ) S25FL256SAGNFI001 to SDRAM AS4C16M16SA-6TIN . I think that i need to use DMA2D peripheric but i am not sure .
my tft LCD is :
/external-link.jspa?url=http%3A%2F%2Fwww.buydisplay.com%2Fdefault%2F7-inch-lcd-module-capacitive-touch-screen-panel-i2c-spi-serial
Thanks
#memory #qspi #sdram #flash2017-04-22 4:36 AM
Display driver with touch support has an SPI interface and the controller has its own internal frame buffer.
It's a difficult question because it depends on what type of graphics library will be used and at what refresh rate the video frame will change (video movies?) and if mostly the whole screen is refresh or mostly partial rectangle areas... motion artifacts (double buffer with swap on Vblank)
So the answer might be 'it depends' especially if the display controller has drawing primitives by HW commands...
2017-04-22 4:44 AM
Duplicate Thread
https://community.st.com/0D50X00009XkXvLSAV