cancel
Showing results for 
Search instead for 
Did you mean: 

How to use the boot0 pin as analog input

zl.1
Associate

I use the STM32CUBEMax configure PB8(boot0)pin as analog input ,but I can not find any message to connect the input channel with the ADC module

1 REPLY 1
Petr DAVID
ST Employee

Hello zl.1,

welcome to ST community. What MCU are you using and what will be the PIN function. The Analog_mode is related GPIO mode for selected pin. You should see similar in option for your MCU as pictured in the screenshot below:

0693W00000APHMJQA5.png

Let me know if that is what you were looking for. And you can also click on Select as Best as it will make it easier for other community members to distinguish this question from unanswered ones.