cancel
Showing results for 
Search instead for 
Did you mean: 

How to unlock STM32G031J6M6 (STM32G0316-DISCO)?

spacemishka
Associate II

Hi,

today i got a STM32G0316-DISCO and totally forgot to setup serialwire. All Pins except PIN6 where configured as GPIO-Output. No i can't connect to the MCU. I tried most of the hints regarding "connect under reset" but no success. I had also one try with my J-Link, but no success. Is it possible to use JTAG to get it back working?

thanks

Peter

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief III
2 REPLIES 2
MM..1
Chief III

Try disconnect and connect Idd jumper with connection attempt

read [SOLVED] STM32G031J6-DISCO Can no longer program the chip (“No device found on target�?)

spacemishka
Associate II

thanks....that worked