2019-11-03 11:57 PM
I am using STM32CubeIDE to generate a code and want to transmit two different data(voltage and temperature of battery) serially . I am able to transmit single data at a time means i am able to check voltage or temperature individually but when i am trying to send both the data simultaneously ,facing some problems like it reads only one data or getting data of voltage and temperature alternately .But i want to get separate data for further use. Please give me any suggestion.
2019-11-04 3:53 AM
Hi. Add some markers to your transmission packet. For example, packet can be: 0xAA, TempL, TempH, 0xBB, VolL, VolH. So you can handle markers and find out what data type follow after it.
2019-11-04 7:18 PM
Thanks for your response sir,as you said that add some markers in transmission packet then it will not be a syntax error of transmission? I mean in transmit i can send only five parameters, so how can i add 6th one?