How to transmit data using RS485 with uart?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-05-16 7:19 AM
Hi everyone,
I'm trying to transmit and receive data through rs485 with uart. Using Uart with DMA in normal mode and referance from this project.
https://controllerstech.com/rs485-module-and-stm32/
However, in this project there are 2 different stm. I want to use 1 stm 2 uarts and 2 module. Therefore I combine these two codes. It writes SEND to tx buffer but neither transmit nor receive. When I check serial port to see data, only 00 or null
void dataSend (uint8_t *data)
{
if(huart.Instance == UART1)
{
HAL_GPIO_WritePin(UART1_EN_GPIO_Port, UART1_EN_Pin, 1);
HAL_UART_Transmit_DMA(&huart1, (uint8_t*)rx1_buffer, rx_buff);
HAL_GPIO_WritePin(UART1_EN_GPIO_Port, UART1_EN_Pin, 0);
}
else if(huart.Instance == UART2)
{
HAL_GPIO_WritePin(UART2_EN_GPIO_Port, UART2_EN_Pin, 1);
HAL_UART_Transmit(&huart2, rx2_buffer, sizeof(rx_buff),1000);
HAL_GPIO_WritePin(UART2_EN_GPIO_Port, UART2_EN_Pin, 0);
}
}
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
{
if(huart->Instance == USART1)
{
HAL_UARTEx_ReceiveToIdle_DMA(&huart1, rx1_buffer, rx_buff);
}
else if(huart->Instance == USART2)
{
rx3_buffer[0] = "F";
rx3_buffer[1] = "P";
rx3_buffer[2] = "G";
rx3_buffer[3] = "A";
dataSend(rx2_buffer);
HAL_UARTEx_ReceiveToIdle_DMA(&huart2, rx2_buffer, rx_buff);
}
}
int main()
{
HAL_UARTEx_ReceiveToIdle_DMA(&huart1, rx1_buffer, rx_buff);
HAL_Delay(100);
HAL_UARTEx_ReceiveToIdle_DMA(&huart2, rx2_buffer, rx_buff);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
sprintf(tx1_buffer, "SEND %d",indx++);
dataSend(tx1_buffer);
HAL_Delay(100);
}
}
Labels:
- Labels:
-
UART-USART
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0