cancel
Showing results for 
Search instead for 
Did you mean: 

How to spot counterfeit or second-hand STM32F405RG MCUs?

Stefan Hamminga
Associate III

I designed a board for a client using the STM32F405RGT6. The first batch worked fine, but once the client ordered another batch of boards none of them worked. The used MCU has different markings. A quick image search in Google shows the style of markings on the non-working MCUs are used, but it might be an older style? The difference is mainly in the bottom row layout.

Is there an official guideline for what the correct markings should be and how to detect if an MCU has been used before?

3 REPLIES 3
Stefan Hamminga
Associate III

Update: I got some pictures of each MCU type. The newer boards seem to have a revision 2 IC, the older ones a revision 4. The date code seems to indicate the problem MCUs are at least 6 years old?

This is the MCU on the second (later) batch of boards, not working:

0693W00000BbdAcQAJ.jpg 

By comparison this is the MCU on the first batch of boards:

0693W00000BbdAXQAZ.jpg

Let's just assume for start, the mcus in second batch are also OK, but there's some other problem.

Try to be specific in "doesn't work".

Can you program the chips using SWD? If you run some simple trivial blinky, does it run?

JW

TDK
Guru

The datasheet will have details on marking.

0693W00000BbfRkQAJ.png 

The top picture looks more like the marking I've come to expect.

If you feel a post has answered your question, please click "Accept as Solution".