cancel
Showing results for 
Search instead for 
Did you mean: 

How to run HRTIM DMA to GPIO?

TSchi.3
Associate

Hey Community,

i am working on a parallel output interface. I want to realize it with GPIOE and all of the 16 Pins.

To Generate an output i used TIM2 to trigger DMA1 so far so good. The Output is working with memory to peripheral. The DMA is copying the databytes from the SRAM into the GPIOE->ODR Register (fmax=24MHz). Now i want to use HRTIM to generate the DMA request for more precise and faster Output.

I could not get it to run. Here my Code:

ALIGN_32BYTES(__attribute__((section (".sram1_s0"))) uint32_t msg2[]) =
{
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000),
		((uint16_t)0x0100),((uint16_t)0x0000) 
 
};
 
void New_HRTIM(void){
 
	__HAL_RCC_DMA1_CLK_ENABLE();
	__HAL_RCC_DMA2_CLK_ENABLE();
	__HAL_RCC_HRTIM1_CONFIG(RCC_HRTIM1CLK_CPUCLK);
	__HRTIM1_CLK_ENABLE();
 
	hhrtim1.Instance = HRTIM1;
	hhrtim1.Init.HRTIMInterruptResquests = HRTIM_IT_NONE;
	hhrtim1.Init.SyncOptions = HRTIM_SYNCOPTION_NONE;
 
	HAL_HRTIM_Init(&hhrtim1);
 
	  HRTIM_TimerCfgTypeDef pTimerCfg = {0};
 
	  pTimerCfg.InterruptRequests = (HRTIM_MASTER_IT_NONE  | HRTIM_TIM_IT_NONE);
	  pTimerCfg.DMARequests = HRTIM_TIM_DMA_RST; 
	  pTimerCfg.DMASrcAddress = (uint32_t)&msg2;
	  pTimerCfg.DMADstAddress = (uint32_t)&(GPIOE->ODR);
	  pTimerCfg.DMASize = sizeof(msg2);
 
	  pTimerCfg.HalfModeEnable = HRTIM_HALFMODE_DISABLED;
	  pTimerCfg.StartOnSync = HRTIM_SYNCSTART_DISABLED;
	  pTimerCfg.ResetOnSync = HRTIM_SYNCRESET_DISABLED;
	  pTimerCfg.DACSynchro = HRTIM_DACSYNC_NONE;
	  pTimerCfg.PreloadEnable = HRTIM_PRELOAD_DISABLED;
	  pTimerCfg.UpdateGating = HRTIM_UPDATEGATING_INDEPENDENT;
	  pTimerCfg.BurstMode = HRTIM_TIMERBURSTMODE_MAINTAINCLOCK;
	  pTimerCfg.RepetitionUpdate = HRTIM_UPDATEONREPETITION_DISABLED;
	  pTimerCfg.PushPull = HRTIM_TIMPUSHPULLMODE_DISABLED;
	  pTimerCfg.FaultEnable = HRTIM_TIMFAULTENABLE_NONE;
	  pTimerCfg.FaultLock = HRTIM_TIMFAULTLOCK_READWRITE;
	  pTimerCfg.DeadTimeInsertion = HRTIM_TIMDEADTIMEINSERTION_DISABLED;
	  pTimerCfg.DelayedProtectionMode = HRTIM_TIMER_A_B_C_DELAYEDPROTECTION_DISABLED;
	  pTimerCfg.UpdateTrigger = HRTIM_TIMUPDATETRIGGER_NONE;
	  pTimerCfg.ResetTrigger = HRTIM_TIMRESETTRIGGER_NONE;
	  pTimerCfg.ResetUpdate = HRTIM_TIMUPDATEONRESET_DISABLED;
	  if (HAL_HRTIM_WaveformTimerConfig(&hhrtim1, HRTIM_TIMERINDEX_TIMER_A, &pTimerCfg) != HAL_OK)
	  {
	    Error_Handler();
	  }
	  __HAL_HRTIM_ENABLE(&hhrtim1, HRTIM_TIMERUPDATE_A);
	  HAL_HRTIM_WaveformOutputStart(&hhrtim1, (HRTIM_OUTPUT_TA1 | HRTIM_OUTPUT_TA2));
	  HAL_HRTIM_WaveformCounterStart_DMA(&hhrtim1,HRTIM_TIMERID_TIMER_A);
	  HAL_HRTIM_UpdateEnable(&hhrtim1, HRTIM_TIMERUPDATE_A);
 
	  ConsolePrintUsart3("while start..");
	  int i = 0;
	  while(1) {
		  i += 1;
	    
	  }
 
}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0