2010-07-13 12:08 AM
How to remove NAND flash disk from Mass Storage Demo?
2011-05-17 4:58 AM
Hi!
These names are in file scsi_data.c You have two ways to remove the NAND disk from demo, 1. Study the codes through, then you will know what to remove. 2. Remove the files fsmc_nand.c/h from demo first and rebuild the project, let the compiler tells you what is missing and remove it. Repeatly doing this until there is no errors:-)2011-05-17 4:58 AM
The ''#define MAX_LUN 1'' in file mass_mal.h is a dummy. Instead, modify the variable ''Max_Lun'' in file usb_prop.c. If your project works on NAND and SD both, just change this variable to 0 is enough to make PC sees only the SD and it will work(no reason not to).
2011-05-17 4:58 AM
> These names are in file scsi_data.c
Thanks for that. I used CTRL+F function for finding it, but it is in: 'S', 'T', 'M', ' ', ' ', ' ', format, so I was unsuccessful. > You have two ways to remove the NAND disk from demo, > 1. Study the codes through, then you will know what to remove. > 2. Remove the files fsmc_nand.c/h from demo first and rebuild the project, let the compiler tells you what is missing and remove it. Repeatly doing this until there is no errors:-) The problem is, that even if I remove all the functions connected with NAND, there will be two disks in PC. I need to find where it is configured to use two disks for mass storage demo and change it to one. I already removed the NAND functions. I even do not have the NAND chip on my own hardware, but in PC there are still two disks :( I tried to change the: #define MAX_LUN 1 to #define MAX_LUN 0 in mass_mal.h there was only one disk in PC, it was only SD card (lucky), but the SD card was not working properly. I wasn't able to read and write to the SD card without error.2011-05-17 4:58 AM
>The ''#define MAX_LUN 1'' in file mass_mal.h is a dummy. Instead, modify the variable ''Max_Lun'' in file usb_prop.c. If your project works on NAND and SD both, just change this variable to 0 is enough to make PC sees only the SD and it will work(no reason not to).
I changed ''#define MAX_LUN 0'' in file mass_mal.h as well as ''Max_Lun'' in file usb_prop.c. Now it works without problem. Thanks for advice. Just to complete the information where are stored the string information about USB device: it is in scsi_data.c as well as in usb_desc.c