cancel
Showing results for 
Search instead for 
Did you mean: 

interfacing external RAM with STM32F103ZET6

kashif
Associate II
Posted on July 13, 2010 at 08:32

interfacing external RAM with STM32F103ZET6

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
kashif
Associate II
Posted on May 17, 2011 at 13:58

i am still trying to understand these examples. some confusing points are:

1) what is the difference between ''Default startup'' and ''startup_stm32f10x_hd.s''?

2) what is the difference between ''Default Script File'' and ''stm32f10x_flash_extsram.ld'' ?

3) where i can find this ''Default Script File''?

please help me with your valuable experience and expertise.

regards.

stforum2
Associate II
Posted on May 17, 2011 at 13:58

All in main():

#define SRAM_BASE 0X68000000

short ch;

main()

{

    // use the Wizards (see Wizards menu) to configure the on-chip peripherals

    // later or alternatively right mouse click on a source code view to access an alternative interface to the Wizards

    //{{EDS_CONFIG(PORTS)

    g_pRCC->APB2ENR |= IOPDEN;

    g_pGPIOD->CRH &= ~0XFFFFFFFF;

    g_pGPIOD->CRH |= 0XBBBBBBBB;

    g_pGPIOD->CRL &= ~0X00FF00FF;

    g_pGPIOD->CRL |= 0X00BB00BB;

    g_pRCC->APB2ENR |= IOPEEN;

    g_pGPIOE->CRH &= ~0XFFFFFFFF;

    g_pGPIOE->CRH |= 0XBBBBBBBB;

    g_pGPIOE->CRL &= ~0XF00000FF;

    g_pGPIOE->CRL |= 0XB00000BB;

    g_pRCC->APB2ENR |= IOPFEN;

    g_pGPIOF->CRH &= ~0XFFFF0000;

    g_pGPIOF->CRH |= 0XBBBB0000;

    g_pGPIOF->CRL &= ~0X00FFFFFF;

    g_pGPIOF->CRL |= 0X00BBBBBB;

    g_pRCC->APB2ENR |= IOPGEN;

    g_pGPIOG->CRH &= ~0X00000F00;

    g_pGPIOG->CRH |= 0X00000B00;

    g_pGPIOG->CRL &= ~0X00FFFFFF;

    g_pGPIOG->CRL |= 0X00BBBBBB;

      //}}EDS_CONFIG

    //{{EDS_CONFIG(FSMC)

    g_pRCC->AHBENR |= FSMCEN;

    g_pFSMC->BCR3 = WREN | MWID0;

    g_pFSMC->BCR3 |= MBKEN;

    //}}EDS_CONFIG

    short* p = (char*)SRAM_BASE;

    for (int i = 0; i < 100; i++)

    {

        *p = i;

        ch = *p;

    }

    while (1)

    {

    }

}

kashif
Associate II
Posted on May 17, 2011 at 13:58

thanks Crossware for your reply.

i have already done that using example code 

C:\Program Files\Raisonance\Ride\lib\ARM\STM32Lib-v312\Project\STM32F10x_StdPeriph_Examples\FSMC\SRAM_DataMemory 

using these files in the template project but no success. i an getting the value of TabAddr = 0xFFFFFFFF and MSPValue = 0xFFFFFFF8 , which is not correct.

i don't know what is wrong with the project. it might be the issue of startup file....

kashif
Associate II
Posted on May 17, 2011 at 13:58

i have attached my project folder. it is a template project present in 

C:\Program Files\Raisonance\Ride\lib\ARM\STM32Lib-v312\Project\Template\RIDE

and i have used the example code of

C:\Program Files\Raisonance\Ride\lib\ARM\STM32Lib-v312\Project\STM32F10x_StdPeriph_Examples\FSMC\SRAM_DataMemory

can anybody please verify it and tell me what i am missing in this project. whereas i have successfully used other example codes with this template project.