How to receive data by using SPI communication ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-06 1:33 AM
I use the STM32Lo538 disco board, and this board is connected to one sensor. Moreover, the protocol of this sensor is SPI. I faced difficulties receiving the data from the sensor. When I watched the waveform of this sensor, I noticed that the CS pin was driven from high to low, but data was not received by the master. Furthermore, I checked every possible condition, but still, data is not received by the master. However, I also tried the NSS pin, but this time I am only able to read one register and cannot read another register. What should I do?
CODE :-
void max30001_cs_pin_reset(){
HAL_GPIO_WritePin(BSP_MAX30001_NSS_PIN_GPIO_Port, BSP_MAX30001_NSS_PIN_Pin,
GPIO_PIN_RESET); // Set chip select low
// HAL_GPIO_WritePin(BSP_MAX30001_CS_PIN_GPIO_Port, BSP_MAX30001_CS_PIN_Pin,
// GPIO_PIN_RESET); // Set chip select low
}
void max30001_cs_pin_set() {
HAL_GPIO_WritePin(BSP_MAX30001_NSS_PIN_GPIO_Port, BSP_MAX30001_NSS_PIN_Pin,
GPIO_PIN_SET); // Set chip select high
// HAL_GPIO_WritePin(BSP_MAX30001_CS_PIN_GPIO_Port, BSP_MAX30001_CS_PIN_Pin,
// GPIO_PIN_SET); // Set chip select high
}
int32_t BSP_SPI1_Read(uint8_t *tx_buff, uint16_t tx_size, uint8_t *rx_buff,
uint16_t rx_size) {
HAL_StatusTypeDef ret = HAL_ERROR;
max30001_cs_pin_reset();
HAL_Delay(100);
ret = HAL_SPI_TransmitReceive(&hspi1, tx_buff, rx_buff, rx_size, 500);
if (ret == HAL_OK) {
max30001_cs_pin_set();
HAL_Delay(100);
return ret;
}
return ret;
}
int32_t BSP_SPI1_write(uint8_t *tx_buff, uint16_t tx_size, uint8_t *rx_buff,
uint16_t rx_size) {
HAL_StatusTypeDef ret = HAL_ERROR;
max30001_cs_pin_reset();
HAL_Delay(100);
ret = HAL_SPI_Transmit(&hspi1, tx_buff, tx_size, 100);
if (ret == HAL_OK) {
max30001_cs_pin_set();
HAL_Delay(100);
return ret;
}
return ret;
}
- Labels:
-
SPI
-
STM32L0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-06 7:04 PM
Do you see SCK toggling when oscilloscope probing?
Does the number of clock pulse match the number of data bits transferred? Is the slave working in SPI 4 or 3 wires SPI mode ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-06 9:44 PM - edited ‎2023-11-20 3:51 AM
Yes, the number of clock pulses matches the number of data bits transferred , but sometimes not all the times .
slave is working in SPI 4 wire. My slave is the MAX30001 sensor, and this sensor is connected to the STM32 with the level shifter and buck converter because this sensor requires 1.8 volts.
figure , which is mentioned below has some change D3 line is basically MOSI and D1 line is CLK
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-06 9:59 PM
can I use HAL_SPI_Deint() , while using NSS pin ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-06 10:29 PM
As you use SPI 4 wires, it is better to consider that using SPI_TransmitReceive() function.
Extra dummy TX data to get all the needed clock bits (for reading), and RX buffer should be as big as TX buffer. If the transaction is 2 bytes to send and 8 bytes to read, make 2 buffers of 10+ bytes and use both buffer in the TransmitReceive function.
NSS is a pure GPIO not related to SPI, controlled by SW, in master mode (at least the way I use it).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-06-08 3:45 AM
so I use CS pin now instead of NSS pin ?
I tried to control NSS pin by using SW but It is not controlled
can you please give me idea how to do this thing ?