How to place some part of code in ITCM and DTCM in stm32h745 ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-09-09 9:37 PM
Hi ,
I am using stm32h745 and I am new to this dual core processor. I have some doubts with this processor access:
1)Do both the processors mutually controllable i.e., can we start and stop cortex M4 using cortex M7 and vice versa .. ?
2)I want to place some part of code in the ITCM and DTCM ,and here my question is that how can I configure this ITCM and DTCM and place some part of my code in ITCM and DTCM.
Thanks and regards,
Parvathi.P
- Labels:
-
Flash
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-09-09 10:24 PM
Typically you'd use the link script or scatter file to describe the regions/sections, make the code and data with __attributes__ ((section(.xyz))) and have startup or scatterloader code to copy the pieces in place.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-09-25 11:37 PM
/* used by the startup to initialize data */
_siitcmram = LOADADDR(.itcmram);
.itcmram :
{
. = ALIGN(4);
_sitcmram = .; /* create a global symbol at data start */
*(.itcmram) /* .data sections */
*(.itcmram*) /* .data* sections */
*Src/stm32h7xx_it.o(.text .text*)
*Drivers/STM32H7xx_HAL_Driver/Src/*.o(.text .text*)
*Middlewares/Third_Party/FreeRTOS/Source/*.o(.text .text*)
*Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F/port.o(.text .text*)
*Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS/cmsis_os.o(.text .text*)
*Middlewares/Third_Party/FreeRTOS/Source/portable/MemMang/*.o(.text .text*)
. = ALIGN(4);
_eitcmram = .; /* define a global symbol at data end */
} >ITCMRAM AT> FLASH
Linker script place whole C files to the ITCM section.
Now your startup file has to copy the code from the Flash to the ITCM RAM.
/**
* @brief This is the code that gets called when the processor first
* starts execution following a reset event. Only the absolutely
* necessary set is performed, after which the application
* supplied main() routine is called.
* @param None
* @retval : None
*/
.section .text.Reset_Handler
.weak Reset_Handler
.type Reset_Handler, %function
Reset_Handler:
/* Enable SRAM clocks early */
ldr r0,=0x580244dc
ldr r3,[r0]
orr r3, r3, #3758096384 /* 0xE0000000 */
str r3,[r0]
ldr sp, =_estack /* set stack pointer */
/* Copy the data segment initializers from flash to SRAM */
movs r1, #0
b LoopCopyDataInit
CopyDataInit:
ldr r3, =_sidata
ldr r3, [r3, r1]
str r3, [r0, r1]
adds r1, r1, #4
LoopCopyDataInit:
ldr r0, =_sdata
ldr r3, =_edata
adds r2, r0, r1
cmp r2, r3
bcc CopyDataInit
movs r1, #0
b LoopCopyDataInitITCM
/* Zero fill ITCM ram section with source code */
CopyDataInitITCM:
ldr r3, =_siitcmram
ldr r3, [r3, r1]
str r3, [r0, r1]
adds r1, r1, #4
LoopCopyDataInitITCM:
ldr r0, =_sitcmram
ldr r3, =_eitcmram
adds r2, r0, r1
cmp r2, r3
bcc CopyDataInitITCM
ldr r2, =_sbss
b LoopFillZerobss
/* Zero fill the bss segment. */
FillZerobss:
movs r3, #0
str r3, [r2], #4
LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss
/* Call the clock system intitialization function.*/
bl SystemInit
/* Call static constructors */
bl __libc_init_array
/* Call the application's entry point.*/
bl main
bx lr
.size Reset_Handler, .-Reset_Handler