cancel
Showing results for 
Search instead for 
Did you mean: 

How to obtain a Burst Write and/or read of external PSRAM

MDi L.9
Associate

I think the configuration is OK but I don't know how to have a burst Write and/or Read operation.

My goal is to have the fastest possible data transfer with a burst lenght of 128 bytes.

Having a look at HAL I can't identify the correct function to be used and I can't find any AN or Example that use burst transfers.

Any help is welcome.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User

Bursts are enabled by setting FSMC/FMC_BCRx.BURSTEN for read, and FSMC/FMC_BCRx.CBURSTRW for write.

The FSMC/FMC chapters in RMs are not very concisely written so you might need to experiment with your particular memory.

JW

MDi L.9
Associate

Hi JW.

Thank you for your answer.

So, if I understood correctly: as

soon as the FMC is correctly configured any access to that memory area should

be managed through a burst read and/or write.

No need to use special function to

achieve it.

Is it correct?

I will check my initialization and

go on with few tests in the next days.

Thanks, and regards

Maurizio