cancel
Showing results for 
Search instead for 
Did you mean: 

how to measure force of motor

LOGU
Associate II

i need to measure force of a motor but i don't know i how to measure .

please any one help me

i'm using 24v dc motor with encoder

and stm32f446re controller

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
MPast.1
Senior II

Hi LOGU,

to measure the force of a motor you must measure the corrent absorbed from it.

You can use a shunt and an OPAMP to converte the current into a voltage readable from ADC of your microcontroller.

The current flow through the shunt is the same of motor current: this is proportional to the mechanical strength avialable on the shaft.

(encoder is used only to evaluate the speed and direction of rotation).

Best regards

LOGU
Associate II

MPast.1

thanks for your valuable point

i will check.

Best regards