2021-10-18 9:48 PM
Hi there,
I had experience in IAR before, but many of its functionality I dont know well.
Currently I am working with customized ST32F103 board.
In my F/W code says,
Under a function its called,
void OnDSP_GetStatus(WORD *pWord)
{
BOOL bUpdateDSP;
float *pFloat;
long *pErr;
WORD Index;
WORD Size;
then defined a variable like,
pFloat = &pFloat[Size];
pErr = (long*)pFloat;
Again, a related variables are defined as,
g_DSP[ERROR_CODE] = pFloat[0];
g_ErrCode = *((UINT*)& g_DSP[ERROR_CODE]);
if(g_DSP[ERROR_CODE]) SendMessage(MS_ERROR, *((uint32_t*)&g_DSP[ERROR_CODE]));
if(*pErr) SendMessage(MS_ERROR, *pErr);
else g_ErrCode = g_ErrCode & (UINT)((1 << ERRCODE_REMOTE_NOT_CONNECT));
}
My question is how can I see the register value of g_ErrCode and ERRCODE_REMOTE_NOT_CONNECT ( defined in register file)
Very similar to this video, Advanced Debugging Breakpoints in the IAR Embedded Workbench - YouTube