2019-05-24 02:33 AM
interface STM32L151QD with MX25R6435F flash memory using SPI. But i found clock frequency of STM = 32MHz maximum and Flash mem frequency = 80MHz . so how to implement SPI interface between these two. Is it possible??? Do we have any example code???
2020-10-06 03:23 AM
Hi,
Can you share your implementation using the GPIO ?
I have the same problem using SPI.
Thanks,
Mikes
STM32F7