cancel
Showing results for 
Search instead for 
Did you mean: 

how to interface 16x2 LCD to stm32 ? and programm.

kalpeshpatil102
Associate III
Posted on October 12, 2016 at 11:06

hi, i want to interface stm32f0 to 16x2 LCD display. i didn't get good information or tutorial.

i am using keil uv5 and cube mx. please guide me.

thank you .
2 REPLIES 2
Walid FTITI_O
Senior II
Posted on October 12, 2016 at 14:00

Hi patil.kalpesh, 

You may heck the following application note used for a 16x2 HD44780 LCD to get inspired:

http://www.st.com/content/ccc/resource/technical/document/application_note/07/1a/31/66/f9/8e/46/d3/DM00046039.pdf/files/DM00046039.pdf/jcr:content/translations/en.DM00046039.pdf

''Interfacing an HD44780 2-line LCD display

with the STM8SVLDISCOVERY''

The recent official library release are using the TFT LCD .

You can get help from other threads in the forum that discuss the same subject. Make a quick research bu taping for example ''16x2 LCD''.

-Hannibal-
kalpeshpatil102
Associate III
Posted on October 14, 2016 at 13:05

thank hannibal