cancel
Showing results for 
Search instead for 
Did you mean: 

How to implement MODBUS protocol communication using UART in STM32L151RCT6 MCU

MBhir.11
Associate III

Hi,

I am using the STM32L151RCT6 in STM32cube IDE, i need to create MODBUS protocol communication between MCU and other board as slave..

Please suggest me any related link for implement this..

it will be helpful for me...

This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13

HI,

I am trying to pass float value from the MODBUS.

requirement is like i need to read adc data and after that i am converting it into voltage which is of float value .

That float value i need to map in MODBUS holding register and need to pass the float values from Modbus..

I am not getting how to manage the floats in the MODBUS register map , how to read float values from holding register and send???

Can you help me to fix this issue?

You don't have to worry about the mantissa and the exponent. Treat a float as a 4-byte integer by changing its type. In C language it is referred as type casting. An example is given below.

float x,y;

unsigned short int register1,register2;

register1= (unsigned short int)((unsigned int)x & 0xFFFF0000) >> 16; //(16 bit MSB)

register2= (unsigned short int)((unsigned int)x & 0x0000FFFF); //(16 bit LSB)

To recreate the float number, do the following:

y =(float) (((unsigned int)register1<<16) | (unsigned int)register2);

In my opinion this should work, but I haven't checked it out.

In (unsigned int)x casting a float to integer will get an integer part of float value. One can get a binary value by using address of a variable with ((uint16_t*)&x)[0] and ((uint16_t*)&x)[1] . But even better is a union type, which is dedicated for such purposes:

https://stackoverflow.com/questions/26012374/convert-one-32bit-float-number-into-two-16bit-uint-number-and-then-convert-back

saishiva
Associate

basically my sensor is 7  in 1 soil sensor to read the sensor data i am using the rs485 so at first i used to arduino it was worked so i need some support for interfacing the sensor for the stm32 b-l475e-iot01a ,where the sensor working on the modbus portocol