cancel
Showing results for 
Search instead for 
Did you mean: 

How to Generate PWM Signal on IKS4A1 Using MEMS-studio?

Kalam
Associate

Hi, I’m working with the IKS4A1 Nucleo expansion board and F401RE. I need to generate a PWM signal on INT pin 2. The documentation I found focuses on connecting the IKS4A1 with MEMS Studio, and I couldn’t find guidance on configuring PWM signals in MEMS Studio.

Is it possible to configure the PWM signal in MEMS Studio, or do I have to use CubeIDE instead? Any guidance or resources would be greatly appreciated!

1 REPLY 1
Federica Bossi
ST Employee

Hi @Kalam ,

This is not possible in MEMS Studio, only in CubeIDE.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.