How to flush cache in CubeF7 Flash EraseProgram example?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-09-06 8:18 AM
In the CubeF4 Flash EraseProgram example (STM32F4-Discovery/Examples/FLASH) there is this section after the erase:
/* Note: If an erase operation in Flash memory also concerns data in the data or instruction cache,
you have to make sure that these data are rewritten before they are accessed during code
execution. If this cannot be done safely, it is recommended to flush the caches by setting the
DCRST and ICRST bits in the FLASH_CR register. */
__HAL_FLASH_DATA_CACHE_DISABLE();
__HAL_FLASH_INSTRUCTION_CACHE_DISABLE();
__HAL_FLASH_DATA_CACHE_RESET();
__HAL_FLASH_INSTRUCTION_CACHE_RESET();
__HAL_FLASH_INSTRUCTION_CACHE_ENABLE();
__HAL_FLASH_DATA_CACHE_ENABLE();
In the same example in CubeF7 (STM32F769I-Discovery/Examples/FLASH), there is the same note, but before the erase and with no code at all:
/* Note: If an erase operation in Flash memory also concerns data in the data or instruction cache,
you have to make sure that these data are rewritten before they are accessed during code
execution. If this cannot be done safely, it is recommended to flush the caches by setting the
DCRST and ICRST bits in the FLASH_CR register. */
if (HAL_FLASHEx_Erase(&EraseInitStruct, &SECTORError) != HAL_OK)
{
In the examples for other stm32f7 boards there is no note at all... Is there some flush necessary for the stm32f7 or is this note just a copy paste error?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-24 7:48 AM
Any updates on this topic?
I ran into the same issue.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-06-24 9:49 AM
Yes, you're going to have to manage cache-coherency. All the stuff you learned about cache architecture would be prescient here. Review CM7 TRM.
You'd honestly do better doing flash work while the cache isn't enabled, or setting the MPU up to exclude the area in question.
If you do a blanket cache invalidate you'll likely crash the system.
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
‎2024-04-01 3:24 PM
For stm32f7:
Information i have to go by on is:
HAL_StatusTypeDef HAL_Init (void )
This function is used to initialize the HAL Library; it must be the first instruction to be executed in the main program (before to call any other HAL function), it performs the following: Configure the Flash prefetch, and instruction cache through ART accelerator.
There is a document:
Cortex®-M7 cache maintenance operations using CMSIS ia in PM0253.
you can look in the file core_cm7.h.
I think these work well with me. You can look at how the drivers work and craft your own.
and
um1905-description-of-stm32f7-hal-and-lowlayer-drivers
look in HAL FLASH Generic Driver section for some info.
This works for stm32f411re example for a flush:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-01 3:30 PM
based on previous info:
for stm32f7 this seams like it would do the trick.
static void flush_caches(void)
{
SCB_EnableICache(); //Invalidate and then enable the instruction cache
SCB_EnableDCache(); //Invalidate and then enable the data cache
}