2021-03-08 09:33 PM
I have to extract the RSSI from scanned packet w.r.t to its device address. I got the RSSI but I am unable to get the actual device address. But in the manual they mentioned that
"Once the scan parameters are set, the device scanning can be enabled. The controller of the scanner devices sends to upper layers any received advertising packets within an advertising report event. This event includes the advertiser address, advertiser data, and the received signal strength indication (RSSI) of this advertising packet."
If anyone familiar with this one can you tell the possibilities?