2009-10-14 10:41 PM
How to exit WFE (Sleep) using Timer ?
2011-05-17 4:26 AM
How must a timer be set up to exit WFE (Sleep) mode on overflow / underflow? Can the timer generate an EVENT to exit sleep or must I use an interrupt? Any examples please? I couldn't find one in the Std Peri Library.
I can set up the timer and generate an interrupt on timer overflow which I can service in a conventional handler. What I can't understand is how to use the WFE or WFI functions with the timer when I don't want an interrupt service - I just want to pause until the timer overflows, do something and then pause again and so on ... For WFE and WFI it looks like the Gcc compiler doesn't understand __WFI() which assembles as __WFI(); F7FFFF1D bl 0x080002C0 and you must use the form __asm(''wfi''); which assembles properly. __asm(''wfi''); BF30 wfi Actually, it turns out you must use a compiler optimisation setting greater than 0 to get the __WFI(); instruction to produce inline code! Otherwise you get a function call. In passing ... anyone understand what ''force_stores'' does in connection with wfi? Also, why would wfi sometimes seem to miss or skip. Using it in a wait (wfi) loop to flash a LED is intermittent even though the interrupt is definitely regular. [ This message was edited by: Omniverous on 16-10-2009 11:30 ]