cancel
Showing results for 
Search instead for 
Did you mean: 

How to control CS independently of SRAM R/W ?

ranran
Senior II
Posted on December 21, 2016 at 20:37

Hello,

We use LCD interface with SM32F4 , with ILITEK 9341.

According to LCD datasheet is it required that CS will be kept active throught several writings of data/control.

But We see that each write of 8-bit word results in changing the CS from IDLE to active and back to IDLE.

Maybe this can explain our failure to make LCD functional.

SRAM configuration:

LCD interface

chip select NE3.

LCD register select: A0

DATA: 8-bit

What can we do to control CS?

I also see the LCD example with STM32F4 demo, which seems to use SSD2119,

and I see that it also make separate write for command and data, so I wander how it works in EVM.

/**

* @brief Writes to the selected LCD register.

* @param LCD_Reg: address of the selected register.

* @param LCD_RegValue: value to write to the selected register.

* @retval None

*/

void LCD_WriteReg(uint8_t LCD_Reg, uint16_t LCD_RegValue)

{

/* Write 16-bit Index, then Write Reg */

LCD_CMD = LCD_Reg;

/* Write 16-bit Reg */

LCD_Data = LCD_RegValue;

}

Thank you!

Ran

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User
Posted on December 21, 2016 at 21:18

According to LCD datasheet is it required that CS will be kept active throught several writings of data/control.

No. In the 8080-style of interface, RD and WR are ANDed (in negative logic) with CS before they are used in the rest of the circuit, so that when both RD and WR are high, CS is ignored.

But you can try - simply don't set the CS (NE3) pin as AF in GPIOx_MODER, rather, set it as GPIO Out. Then, whenever you want to perform accesses the LCD, set that pin low before, and high after the accesses.

JW

Posted on December 22, 2016 at 13:49

Hi JW,

Thank you very much for the helpful comments!

Please see image here:

https://drive.google.com/file/d/0B22GsWueReZTVEMtcEk4d0VHeVk/view?usp=sharing

 

The yellow is CS, and purple WE (write enable)

I think that if both move to high between writings, then it is not good, Right ?

Thanks,

Ran 

Posted on December 22, 2016 at 14:57

As I've said, it should not matter.