how dose function name connect to interrupt address
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-12-13 4:20 AM
hi.
i am writing a code for Exti interrupt and i do that. But i get a qustion .
when we want to use interrupt , I mean when the interrupt happen , then cpu jump to that interrupt address and the function that we write on the IDE will run .
In fact , we write just interrupt name that it name is same with startup function name.
please watch my interrupt code in main:void EXTI9_5_IRQHandler (void){
GPIO_WriteBit(GPIOB, GPIO_Pin_0, Bit_SET);
while(1){
if( EXTI_GetITStatus(EXTI_Line7) == SET){
lcdPutInt(i);
i++;
delay_ms(200);
lcdClear();
}
}
}
and the same name in startup_stm32f10x_hd_vl.s :
DCD EXTI9_5_IRQHandler
PUBWEAK EXTI9_5_IRQHandler
SECTION .text:CODE:REORDER(1)
EXTI9_5_IRQHandler
B EXTI9_5_IRQHandler
how does the function and EXTI9_5_IRQHandler in startup can connect?
i need some explanation about
communication of this activity.
i use stm32f103re and IAR.
so thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-12-13 4:38 AM
The processor expects the interrupt vectors - which are essentially function pointers, telling the processor where to jump when the interrupt occurs - at a fixed address (or in case of Cortex-M3/4/7, at an address given by SCB->VTOR). That assembly code in startup file is a table of function pointers. The linker fills in the actual position of the interrupt code.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-12-13 4:43 AM
As you guessed, it matches by name, so your code just needs to spell it correctly.
The key is in the word 'PUBWEAK', particularly the 'WEAK' part. An entry symbol that is defined as 'weak' can be replaced by another (implicitly 'strong') symbol of the same name, so if no one defines
EXTI9_5_IRQHandler the linker will adopt the 'weak' one
(in the .s file).
Be aware that some linkers seem to do this better than others. I use maybe 4-5 different IDEs in a week, and for some I need to explicitly delete the 'weak' stuff to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-12-13 5:46 AM
And to be more precise, the names of the interrupt function(s) must match exactly. This way, the linker makes the assignment.
The WEAK attribute (or PUBWEAK, as in your Keil asm example) allows exactly two definitions of said symbol.
One is 'weak', and can be overridden with another symbol - your interrupt handler in this case.
This is general toolchain (compiler+linker) workings.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-12-15 1:54 AM
Thanks all.
i understand what you mean.i want to say that is i dont have startup_stm32f10x_hd_vl.s file , how can i used interrupt ?!! where is address of registers ?!i mean for example i want to write a function with different name ,, and i want to connect this function to a interrupt, how can i do that ? which registers can i use to give it address?
For example i have user manual , and i saw the RCC register and i modify the registers for set the stm32 clock.i dont need any defines or somthing like that.
i know that we'll probably use this way , but i want to understand what is happening in code that this event occur.so thanks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-12-15 3:16 AM
I think you need to consult the IAR Workbench documentation.
IAR has it's own startup files and naming conventions, as far as I remember, something like
xxx_cstartup_iar.s
.The 'weak' default handlers are either declared there, or included.