cancel
Showing results for 
Search instead for 
Did you mean: 

How can STM32F446RE connect external SDRAM

Qiyan Li
Associate
Posted on December 04, 2017 at 21:23

The data sheet says there is no FMC on STM32F446RE. Is that means there is no chance to connect external RAM with STM32F446RE?

#stm-32 #external-ram #stm32f446re
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on December 12, 2017 at 08:32

While the datasheet indeed says that, it's more that you simply don't have enough FMC-connected pins on the 64-pin package to make any reasonable connection.

You still can connect a SRAM and simply manually 'bit-bang' the read and write signals. Performance of course will be slow. SDRAM might be possible with a serious amount of hacking, but not practical at all.

There are also serially-connectible (SPI) SRAMs, e.g. from Microchip and ONSemi; again there is surely a need for some programming and some performance loss.

JW