2016-02-08 03:58 AM
I need to communicate with a device that only supports 32-bit SPI transfers. I see that the stm32f4-family only supports 8 and 16 bits. Can I somehow do a hack to make it work?
2016-02-08 04:46 AM
drive CS by software, split data
2016-02-08 05:17 AM
I forgot to mention, the stm32f4-microcontroller is the slave.
2016-02-08 09:45 AM
The SPI bus is synchronous, you'll just get 4x bytes, or 2x half-words per interaction.
2016-02-08 02:23 PM
I don't understand, the SPI->DR register can only hold 2 bytes. So, I guess I would either receive the first 2 bytes in every transmission or the last 2 bytes. The spacing between the 2nd and the 3rd bytes is too small for me to have time to read the SPI->DR register in between. Likewise, I would problems with the data I would send to the master, I guess I would sent the same 2 bytes twice.
2016-02-08 04:19 PM
The data is buffered, the DR is not the shift register, so TXE will assert as soon as the DR moves to the shift register, and the first bit leaves. You have 16 clock cycles to replenish the DR in 16-bit mode, there is no inter-symbol time. If you don't think you can sustain it manually, use DMA.
Either way, as long as you don't underflow the consecutive 8/16-bit of data will pack back-to-back. With SD cards you're sending thousands of bytes with a continuous clock.