2017-10-02 11:28 AM
Hi,
I try to communicate via CAN. I can transmit data to PCAN but i can't receive in Normal Mode. When i use Loopback, i can receive data. Please Help me.. My configuration is here
/* CAN1 init function */
static void MX_CAN1_Init(void){CAN_FilterConfTypeDef sFilterConfig;
static CanTxMsgTypeDef TxMessage; static CanRxMsgTypeDef RxMessage;/*♯♯-1- Configure the CAN peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
hcan1.Instance = CANx; hcan1.pTxMsg = &TxMessage; hcan1.pRxMsg = &RxMessage;hcan1.Init.TTCM = DISABLE;
hcan1.Init.ABOM = DISABLE; hcan1.Init.AWUM = DISABLE; hcan1.Init.NART = DISABLE; hcan1.Init.RFLM = DISABLE; hcan1.Init.TXFP = DISABLE; hcan1.Init.Mode = CAN_MODE_NORMAL; hcan1.Init.SJW = CAN_SJW_1TQ; hcan1.Init.BS1 = CAN_BS1_6TQ; hcan1.Init.BS2 = CAN_BS2_7TQ; hcan1.Init.Prescaler = 4;if (HAL_CAN_Init(&hcan1) != HAL_OK)
{ /* Initialization Error */ Error_Handler(); }/*♯♯-2- Configure the CAN Filter ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
sFilterConfig.FilterNumber = 0; sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = 0x0000; sFilterConfig.FilterIdLow = 0x0000; sFilterConfig.FilterMaskIdHigh = 0x0000; sFilterConfig.FilterMaskIdLow = 0x0000; sFilterConfig.FilterFIFOAssignment = CAN_FIFO0; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.BankNumber = 0;if (HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig) != HAL_OK)
{ /* Filter configuration Error */ Error_Handler(); }/*♯♯-3- Configure Transmission process ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
hcan1.pTxMsg->StdId = 0x321; hcan1.pTxMsg->ExtId = 0x01; hcan1.pTxMsg->RTR = CAN_RTR_DATA; hcan1.pTxMsg->IDE = CAN_ID_STD; hcan1.pTxMsg->DLC = 2;}
And i use these functions to enable them:
if (HAL_CAN_Receive_IT(&hcan1, CAN_FIFO0) != HAL_OK)
{ /* Reception Error */ Error_Handler(); }//////////////////////////////////////////////////////////////////////////////////////////////////
if (HAL_CAN_Transmit(&hcan1, 10) != HAL_OK)
{ /* Transmission Error */ Error_Handler(); }My MspDeInit functions :
void HAL_CAN_MspInit(CAN_HandleTypeDef *hcan)
{ GPIO_InitTypeDef GPIO_InitStruct;*♯♯-1- Enable peripherals and GPIO Clocks ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* CAN1 Periph clock enable */ CANx_CLK_ENABLE(); / * Enable GPIO clock ****************************************/ CANx_GPIO_CLK_ENABLE();/*♯♯-2- Configure peripheral GPIO ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* CAN1 TX GPIO pin configuration */ GPIO_InitStruct.Pin = CANx_TX_PIN; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Alternate = CANx_TX_AF;HAL_GPIO_Init(CANx_TX_GPIO_PORT, &GPIO_InitStruct);
/* CAN1 RX GPIO pin configuration */
GPIO_InitStruct.Pin = CANx_RX_PIN; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Alternate = CANx_RX_AF;HAL_GPIO_Init(CANx_RX_GPIO_PORT, &GPIO_InitStruct);
/*♯♯-3- Configure the NVIC ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* NVIC configuration for CAN1 Reception complete interrupt */ HAL_NVIC_SetPriority(CANx_RX_IRQn, 2, 0); HAL_NVIC_EnableIRQ(CANx_RX_IRQn);}void HAL_CAN_MspDeInit(CAN_HandleTypeDef *hcan){ /*♯♯-1- Reset peripherals ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ CANx_FORCE_RESET(); CANx_RELEASE_RESET();/*♯♯-2- Disable peripherals and GPIO Clocks ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
/* De-initialize the CAN1 TX GPIO pin */ HAL_GPIO_DeInit(CANx_TX_GPIO_PORT, CANx_TX_PIN); /* De-initialize the CAN1 RX GPIO pin */ HAL_GPIO_DeInit(CANx_RX_GPIO_PORT, CANx_RX_PIN);/*♯♯-4- Disable the NVIC for CAN reception ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
HAL_NVIC_DisableIRQ(CANx_RX_IRQn);}#stm32f72017-10-05 5:03 AM
If using interrupt must to use interrupt sender
// MUST USE THIS LINE OF CODE
while(CAN_busy_check(&hcan1) == 1)HAL_Delay(1);
hcan1.pTxMsg->StdId = 12345;
hcan1.pTxMsg->DLC = 2;hcan1.pTxMsg->Data[0]=1;hcan1.pTxMsg->Data[0]=2;
if(HAL_CAN_Transmit_IT(&hcan1) != HAL_OK)
2017-10-05 5:06 AM
Can init for you 500kbit
static void MX_CAN1_Init(void)
{ hcan1.pTxMsg = &TxMessage1; hcan1.pRxMsg = &RxMessage1; hcan1.Instance = CAN1; hcan1.Init.Prescaler = 5; hcan1.Init.Mode = CAN_MODE_NORMAL; hcan1.Init.SJW = CAN_SJW_1TQ; hcan1.Init.BS1 = CAN_BS1_12TQ; hcan1.Init.BS2 = CAN_BS2_5TQ; hcan1.Init.TTCM = DISABLE; hcan1.Init.ABOM = DISABLE; hcan1.Init.AWUM = DISABLE; hcan1.Init.NART = DISABLE; hcan1.Init.RFLM = DISABLE; hcan1.Init.TXFP = DISABLE; if (HAL_CAN_Init(&hcan1) != HAL_OK) { Error_Handler(); } sFilterConfig1.FilterNumber = 1; sFilterConfig1.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig1.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig1.FilterIdHigh = 0x0000; sFilterConfig1.FilterIdLow = 0x0000; sFilterConfig1.FilterMaskIdHigh = 0x0000; sFilterConfig1.FilterMaskIdLow = 0x0000; sFilterConfig1.FilterFIFOAssignment = 0; sFilterConfig1.FilterActivation = ENABLE; sFilterConfig1.BankNumber = 14; if(HAL_CAN_ConfigFilter(&hcan1, &sFilterConfig1) != HAL_OK)while(1);if(HAL_CAN_Receive_IT(&hcan1, CAN_FIFO0) != HAL_OK) while(1);
hcan1.pTxMsg->StdId = 0x00; hcan1.pTxMsg->ExtId = 0x00; hcan1.pTxMsg->RTR = CAN_RTR_DATA; hcan1.pTxMsg->IDE = CAN_ID_STD; hcan1.pTxMsg->DLC = 8;}
2017-10-05 9:51 AM
Probably NOT 500k in this case.
2017-10-05 9:52 AM
Your settings are almost certainly NOT 1Mbit/s
What is the APB clock for the CAN peripheral?
2017-10-05 4:19 PM
You wont be able to receive anything if ABOM is not set.
to enable automatic bus-off management, set the hcan1.Init.ABOM= ENABLE
to be sure, you should disable the filters too: sFilterConfig1.FilterActivation = DISABLE
to check the final baud rate, transmit something and check the Scope.
I used CubeMx to calculate the baud settings.
I used CanDo hardware to transmit every 10mSec, then I made the receiver work first.
2017-10-05 6:35 PM
>>I used CanDo hardware to transmit every 10mSec, then I made the receiver work first.
Very good advice
>>I used CubeMx to calculate the baud settings.
It's not complicated, and easier than scoping
CAN Rate = ((APBClock / Prescaler) / (x + y + z)) where the sum is of the bit quanta widths
2017-10-05 6:39 PM
its so nice to see the scope running.
You can see if the data is clean, you can check the leading edges, its well recommended.
a 4 channel Color Scope like TDS2024 is a minimum level of scope for a professional engineer.