How are you supposed to use HAL_UART_Receive in STM32Cube ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-25 9:52 AM
I am implementing a command parser that receives data on a serial port. My need is to read one byte at a time and when I recive a full command I will handle it.
I look at the example in STM32Cube_FW_L0_V1.1.0\Projects\STM32L053R8-Nucleo\Examples\UART\UART_TwoBoards_ComPolling\Src\main.c In line 152:if(HAL_UART_Receive(&UartHandle, (uint8_t *)aRxBuffer, RXBUFFERSIZE, 5000) != HAL_OK)
{ Error_Handler(); } I have modified this to lower the timeout value and set RXBUFFERSIZE to 1 and call the function in a loop. However I think the original code is not a good example since if the function HAL_UART_Recive gets timeout the function will return HAL_TIMEOUT and the code will end up in the Error_Handler with a while(1) loop. If just ignoring this by not calling Error_Handler when getting HAL_TIMEOUT and call the function HAL_UART_Recive once more it will return HAL_BUSY. And it seems like no way to get out of this. So I think this example is broken if it would serve as an example on how to use HAL_UART_Receive with a timeout. So if possible if someone could share with me a code snippet where you can read bytes once at a time in a loop from UART with correct error handling I would be happy.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-27 6:39 AM
I ended up with using the stm32snippetsl0 library for doing this. This was much more straightforward.
I think that the STM32Cube library needs more work before you can actually base your work on this.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-28 2:08 PM
/*hotboards.org*/uint8_t RxBuffer[10];
/*Buffer donde se respalda la informacion recivida*/
uint8_t RxByte;
/*Byte de recepcion temporal*/
__IO ITStatus stat = RESET;
/*Bandera que indica si transmisor esta libre*/
UART_HandleTypeDef UartHandle;
/*declaramos estructura tipo uart*/
int
main(
void
)
{
GPIO_InitTypeDef GPIO_InitStruct;
/*declaramos estructura tipo gpios*/
HAL_Init();
/*incializamos libreria cube*/
__GPIOA_CLK_ENABLE();
/*habilitamos reloj del puerto A*/
/*configuramos pin 8, 9 y 10 en modo salida push-pull*/
GPIO_InitStruct.Pin = GPIO_PIN_8 | GPIO_PIN_9 | GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
/*aplicamos configuracion*/
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/*declaramos las opciones para configurar el modulos UART2, 9600 baudrate,
8bits, 1 bit de stop, sin paridad y sin control de flujo */
UartHandle.Instance = USART2;
UartHandle.Init.BaudRate = 9600;
UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
UartHandle.Init.StopBits = UART_STOPBITS_1;
UartHandle.Init.Parity = UART_PARITY_NONE;
UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
UartHandle.Init.Mode = UART_MODE_TX_RX;
UartHandle.Init.OverSampling = UART_OVERSAMPLING_16;
/*inicilizamos uart1 con los parametros anteriores*/
HAL_UART_Init(&UartHandle);
while
(1)
{
if
(HAL_UART_GetState(&UartHandle) == HAL_UART_STATE_READY)
{
/*Receptor esta libre para mnadar interupcion por recepcion*/
HAL_UART_Receive_IT(&UartHandle, &RxByte, 1);
}
if
(stat == SET)
/*llego cadena completa por serial*/
{
stat = RESET;
/*limpiamos la bandera*/
if
(memcmp(
''uno\r''
, RxBuffer,
sizeof
(
''uno\r''
)-1) == 0)
{
/* si fue la palabra led\r invierto led en A8 */
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_8);
}
else
if
(memcmp(
''dos\r''
, RxBuffer,
sizeof
(
''dos\r''
)-1) == 0)
{
/* si fue la palabra led\r invierto led en A9 */
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_9);
}
else
if
(memcmp(
''tres\r''
, RxBuffer,
sizeof
(
''tres\r''
)-1) == 0)
{
/* si fue la palabra led\r invierto led en A10 */
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_10);
}
}
}
}
/*
Funcion callback que respalda los caracteres llegados e informa cuando llego el caracter \r que significa fin de cadena*/
void
HAL_UART_RxCpltCallback(UART_HandleTypeDef *UartHandle)
{
static
uint32_t i = 0;
RxBuffer[i] = RxByte;
/*se respalda dato*/
i++;
/*incremento indice*/
if
(RxBuffer[i-1] ==
'\r'
)
/*fin de cadena?*/
{
stat = SET;
/*activo bandera de cadena completa*/
i = 0;
/*reinicia indice*/
}
}