cancel
Showing results for 
Search instead for 
Did you mean: 

High current draw in STOP mode when RTC Alarm has been used

Thomas Hoppe
Associate III

We have a very weird behavior in a battery powered IoT device. We should have a very low STOP mode current draw of 1.4 uA @ 3 VCC. The problem is, as soon as we use the RTC Alarm just once and although the alarm already fired during NORMAL operation, the current consumption is ~20 uA in STOP mode. The use of the wake up feature of the RTC does not cause this behavior, it's just alarms. Here is an example to reproduce this:

 

// Globals
volatile int alarmVal = 0;
void HAL_RTC_AlarmAEventCallback( RTC_HandleTypeDef *hrtc ) {
alarmVal = 1;
}

// Event Loop
while(1) {
RTC_AlarmTypeDef alarm;
RTC_TimeTypeDef ts;
RTC_DateTypeDef ds;

// Disable Alarm
HAL_RTC_DeactivateAlarm(&hrtc, RTC_ALARM_A); // Disable Interrupt
__HAL_RTC_ALARM_CLEAR_FLAG(&hrtc, RTC_FLAG_ALRAF); // Clear Flag (RTC ALARM A)
__HAL_RTC_ALARM_EXTI_CLEAR_FLAG(); // Clear Flag (EXTI)

// Get Time
do {
HAL_RTC_GetTime(&hrtc, &ts, FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &ds, FORMAT_BIN);
} while(ts.Seconds == 59); // cheat: Increment second without care of real clock

// Set Alarm
alarm.AlarmTime.SubSeconds = ts.SubSeconds; // 210
alarm.AlarmSubSecondMask = 8 << RTC_ALRMASSR_MASKSS_Pos; // 0x8000000
alarm.AlarmTime.Seconds = ts.Seconds + 1; // 27
alarm.AlarmTime.Minutes = ts.Minutes; // 0
alarm.AlarmTime.Hours = ts.Hours; // 0
alarm.AlarmDateWeekDay = ds.WeekDay; // 1
alarm.AlarmTime.TimeFormat = ts.TimeFormat; // 0
alarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE; // 0
alarm.AlarmMask = RTC_ALARMMASK_NONE; // 0
alarm.Alarm = RTC_ALARM_A; // 0x100
alarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE; // 0
alarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET; // 0
HAL_RTC_SetAlarm_IT(&hrtc, &alarm, RTC_FORMAT_BIN);

// Wait Alarm
for(alarmVal = 0; !alarmVal;);
HAL_RTC_DeactivateAlarm(&hrtc, RTC_ALARM_A);
__HAL_RTC_ALARM_CLEAR_FLAG(&hrtc, RTC_FLAG_ALRAF);
__HAL_RTC_ALARM_EXTI_CLEAR_FLAG();

// Stop Mode
HAL_RTC_MspDeInit(&hrtc);
HW_EnterStopMode();
HAL_RTC_MspInit(&hrtc);
}

We are using the LSE clock for the RTC

We have tried multiple ways to de-init the RTC before going to STOP mode but nothing helps.

How can this be explained and resolved?

BG

 

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
KDJEM.1
ST Employee

Hello @Thomas Hoppe ,

The typical current consumption in stop mode depends on the temperature and also on the RTC and Clocks.

  • When the RTC disabled and all clocks OFF the typical current consumption, for VDD=3V, can be ranged between  0,43µA and 12.5 µA  when the temperature range [-40°C 125°C].
  • When the RTC enabled and running on LSE, the typical current consumption increased and becomes range between 1µA and 14.1µA when the temperature range [-40°C 125°C], for VDD=3V.

So, the RTC is related to current consumption in stop mode. For more explanation, please take a look to the datasheet figure 18 and 19.

Thank you.  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @KDJEM.1 , this is not really the point of the problem and the demo I have provided. The point is that after the RTC triggered a wake-up, via Alarm or wake-up timer, the current draw was highly increased (20uA in our case). We have found the cause now which is that clearing of the Interrupt was missed:

--- Core/Src/main.c
+++ Core/Src/main.c
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
if(GPIO_Pin == Button0_Pin)
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
}

void HW_EnterStopMode() {
HAL_ADC_DeInit(&hadc);
HAL_GPIO_WritePin(DC_Conv_Mode_GPIO_Port, DC_Conv_Mode_Pin, GPIO_PIN_RESET); // useful: Disable LEDs, I2C/SPI ICs, from 900 uA

HAL_PWREx_EnableUltraLowPower(); // useful: STOP Mode from 16.3 uA to 870 nA (when RTC ALARM never fired)
HAL_PWREx_EnableFastWakeUp(); // required: To wakeup via [PA0, GPIO_EXTI0, Button0, Button Press]

+ __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); // fixes the 20 uA
__HAL_RCC_PWR_CLK_ENABLE(); // Enable power control clock

hwSlept = 1;
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
HW_ExitStopMode();
}

So with this addition in the demo code, it was solved. Can you confirm that?

KDJEM.1
ST Employee

Hi @Thomas Hoppe ,

Glad to know that the issue is solved and thank you for your sharing the solution this may help other users.

Entering low-power mode through WFI or WFE will be executed only is no interrupt and no event is pending.

Thank you for your contribution.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.