cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, This is Suresh, This my first post in this forum, I am new guy for STM32 Arm chips,

msureshkumar2610
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8

Does Suresh have a question?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

yes. I cant use my stlink and blue pill module, STM32F103C8 (Blue PILL) and STM32F103CB6T(STLINK clone). Driver not properly not installed and also I cant debug and flash my target board.

I got below error

Target not found,

Target core not powered.

SWDIO/SWCLK not correctly connected.

ST-LINK not connected to VTarget and GND.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

3.3 to 3.3

gnd to gnd

swio to io

clk to clk

this is forum also looking great like arduino

thanks for buddy for replying

in india the time is 2:23 AM

And you've measured 3 or 3.3V ?

I'm not using blue pill boards, if it has a USB port you could try pulling the BOOT0 pin high and seeing if will connect in DFU mode. If so you could use the Cube STM32 Programmer application. ​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..