cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I'm utilizing an STM32L443RCT in my design and need to know what a typical 10 pin programming header pinout looks like for the device. Which signals would I need SWDIO, SCLCK etc. to wire to the 10 pin header? Any help would be much appreciated.

WAkba.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
S.Ma
Principal

Have a look also at TAG connect if we are talking of a production board which prefferably for cost, does not use any connector.

Pavel A.
Super User

See UM2502 (the ST-LINKv3 document), Fig 10 on page 19.

It is 14-pin extension of the 10-pin connector. Two pair of pins added on both sides.

As a minimum you'll need SWDIO, SWDCLK, GND and NRST (optional but highly recommended).

​Then you can connect T_VCC, useful to detect the target voltage.

​Then you can connect SWO - or the two extension pins from UART TX, RX on the target to the VCP of the debugger or standalone TTL UART to USB adapter. Either option is very useful.

If the target footprint is tight, consider needle connector (6 or 10 pin variants) - but the adapter cables are obscenely expensive.