2018-01-08 9:23 PM
we have st-link come along with nucleo boards.i want to use same st-link to flash custom stm-boards llike we do with external st-link.is it possible?
2018-01-08 9:42 PM
chapter 6.2.4
It is very easy to use the ST-LINK/V2-1 to program the STM32 on an external application.
Simply remove the two jumpers from CN2 as illustrated in Figure9: Using ST-LINK/V2-1 to program the STM32 on an external application
, and connect the application to the CN4 debug connector according to Ta b l e 5