2020-10-27 3:46 AM
The nucleo ported project doesn't work , i cant understand what could be the issue . I keep getting verification failed error , HAL_TIMEOUT .
The download timeout is 10000U ,changes made to it (50 seconds) how does this impact the code, will it wait for a longer duration to receive packets .
Below are the changes made in my project:
1)Nucleo board does not have an external clock HSE as configured in the original stm32eval hence using HSI clock at 32MHZ freq using pll . will this lead to any problems.
2) used cubemx to generate the nucleo project, just enabled usart and crc .
Apart from the above i have used the same flash_if.c ,y_modem .c,menu.c,common.c files from the example , only changed to the usart i am using.
user application address 0x8004000 , i have also set the same for the app bin file that is generated no mistakes here.
IAP code from 0x08000000 size of code 0x4000 .
using teraterm console(4.105) ,baud rate: 115200 ,ymodem (1K) .
Need advice on this , Thanks in advance.
2020-10-30 7:03 AM
Hello @svii ,
Did you change the User Application vector table offset?
Best Regards,
Mohamed Aymen.
2020-11-02 1:01 AM
Hi thanks for the reply , yes i have changed the user application vector table offset.
2020-11-06 12:27 AM
Hello @svii ,
Just to make sure, did you set the vector table offset of the user application to 0x4000 ?
Best Regards,
Mohamed Aymen.