cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I am looking for some advice about interfacing ads8323 at 500ksps to STM32F427 MCU without using extra hardware (maybe some glue logic) to have the minimum overhead for MCU to gather the data. Thanks!

RAnva.2
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Probably a pretty finite number of those.

Looks like using the FSMC would be the route, perhaps using DMA triggered by a TIM input

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3
Ozone
Principal III

Of course you could connect the digital signals to GPIOs of a MCU.

But I see two issues:

This is a 5V device, you would need levelshifters.

A 500ksps sample rate is easily managed via a serial connection. No commercial project would waste so much pins, and go for a SPI-based ADC instead.

RAnva.2
Associate

Thanks! This is a 16-bit parallel ADC that I need to use but my question is mostly firmware overhead. What is the best way to connect this parallel ADC to STM to have the minimum overhead on firmware. I am asking from experts who used parallel ADCs with STM.

Probably a pretty finite number of those.

Looks like using the FSMC would be the route, perhaps using DMA triggered by a TIM input

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..