2020-06-02 2:33 AM
Please find the code here,
SET_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
LL_OPAMP_SetMode (OPAMP2, LL_OPAMP_MODE_FUNCTIONAL);
LL_OPAMP_SetFunctionalMode (OPAMP2,LL_OPAMP_MODE_STANDALONE);
LL_OPAMP_SetInputNonInverting (OPAMP2, LL_OPAMP_INPUT_NONINVERT_IO0); //PA7
LL_OPAMP_SetInputInverting (OPAMP2, LL_OPAMP_INPUT_INVERT_IO0); //PA5
LL_OPAMP_SetInternalOutput (OPAMP2, LL_OPAMP_INTERNAL_OUPUT_DISABLED); //PA6
LL_OPAMP_Enable (OPAMP2);
2020-06-15 5:14 AM
Post schematics of the connection. What is the expected behaviour and what is the observed one?
JW
2020-06-16 1:49 AM
Hi,
Please find the attached schematic.
Pins OPAMP2_VINP and OPAMP2_VINM are being connected to input pins of MCU Opamp, and I'm trying to measure the output at OPAMP2_VOUT (MCU OPAMP output pin). Also, voltage of around 1.2V (half of VRef of DAC) is being supplied from DAC.
Expected output - Voltage based on diffrential input (I have shunt based currrent measurement circuit preceding this, hence actual input depends on value of current)
Observed output - zero voltage at all cases
Thanks,
Rhushabh
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.