2020-06-14 11:56 PM
As I've seen in cubeMX all periphereals I use match the same pins in both versions of x1 series (which vary just in the absence of AES encryption module) but I cannot find in any datasheet wether they truly are as it is not mentioned anywhere as far as I can tell
2020-06-15 3:38 AM
G431 and G441 are the same die, with crypto disabled on the G431. Pinout is the same, as there is only one datasheet.
2020-06-15 7:41 AM
Well, I am pretty sure that there are 2 datasheets, at least for CB devices
2020-06-16 1:58 AM
There are two datasheet, sorry for my missinformation. But I am sure that both are the same die as they have the same DBGMCU_ID.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.