2020-08-08 5:49 AM
I need to generate:
Do you think that core of this MCU is able fulfill these tasks? Is necessary to choose another one or not.
Thank you very much.
Best Regards,
Miro
2020-08-08 6:41 AM
So, you want 300MHz timers, and 7 individual 2MSps ADCs - yet you are concerned about the processor core?
JW
2020-08-08 7:54 AM
Only the H7 is going to be able to have a 300MHz timer, which is going to be required to do 3MHz at 1% duty cycle. And even then, only with the HRTIM peripheral.
If you are more flexible on the frequency, or the PWM resolution, you will have more options.