cancel
Showing results for 
Search instead for 
Did you mean: 

Hİ Bros, I am trying to read the weight from the HX711 amplifier with the STM32F407VG Development board.

CüneytKüçük
Associate II

I'm following the 'value' variable in the code below from the STM Studio interface. When no pressure is applied, the 'value' variable starts from a fixed number (3.62049). When I apply pressure to the Load-Cell, the digit of this value changes after the comma. How can I fix this. Please help.

CODE:

#include "main.h"

#include "stm32f4xx_hal.h"

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

uint8_t value=0;

uint8_t i = 0;

int32_t adc_value = 0;

int32_t c_value = 0;

uint8_t symb_sel;

uint8_t symbols[10] = {0x3f,0x6,0x5b,0x4f,0x66,0x6d,0x7d,0x7,0x7f,0x6f};

uint8_t s[3];

uint8_t temp;

GPIO_PinState dataadc=GPIO_PIN_SET;

#define pause for(int n=0;n<5;n++){};

int main(void)

{

 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();

 while (1)

 {

 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);

   temp=value;

   s[0]=0;s[1]=0;s[2]=0;

   while (temp>=100){temp=temp-100;s[2]++;}

   while (temp>=10){temp=temp-10;s[1]++;}

   s[0]=temp;

   symb_sel++;

   HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0,GPIO_PIN_SET);

   HAL_GPIO_WritePin(GPIOC, GPIO_PIN_1,GPIO_PIN_SET);

   HAL_GPIO_WritePin(GPIOC, GPIO_PIN_2,GPIO_PIN_SET);

   if(symb_sel>3)symb_sel=1;

   if(symb_sel==1)HAL_GPIO_WritePin(GPIOC, GPIO_PIN_0,GPIO_PIN_RESET);

   if(symb_sel==2)HAL_GPIO_WritePin(GPIOC, GPIO_PIN_1,GPIO_PIN_RESET);

   if(symb_sel==3)HAL_GPIO_WritePin(GPIOC, GPIO_PIN_2,GPIO_PIN_RESET);

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, 0x1&symbols[s[symb_sel-1]]);

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, 0x2&symbols[s[symb_sel-1]]);

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, 0x4&symbols[s[symb_sel-1]]);

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_3, 0x8&symbols[s[symb_sel-1]]);

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, 0x10&symbols[s[symb_sel-1]]);

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, 0x20&symbols[s[symb_sel-1]]);

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, 0x40&symbols[s[symb_sel-1]]);

   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, 0x80&symbols[s[symb_sel-1]]);

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);

  while (HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_15));

  for(i=0;i<24;i++)

  {

  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);

  pause

  adc_value <<= 1;

  if(HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_15))adc_value++;

  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);

  };

  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);

  pause

  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);

  /*HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);

 // pause

  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);

  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);

 // pause

  HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);

  i++;

  };*/

   //while(adc_value>=255)adc_value>>=8;

   c_value=adc_value;

   value=adc_value;

   adc_value=0;

 }

 }

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage

 */

 __HAL_RCC_PWR_CLK_ENABLE();

 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the CPU, AHB and APB busses clocks

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

 RCC_OscInitStruct.HSIState = RCC_HSI_ON;

 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

 RCC_OscInitStruct.PLL.PLLM = 8;

 RCC_OscInitStruct.PLL.PLLN = 192;

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

 RCC_OscInitStruct.PLL.PLLQ = 7;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

Error_Handler();

 }

 /** Initializes the CPU, AHB and APB busses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)

 {

Error_Handler();

 }

}

/**

 * @brief GPIO Initialization Function

 * @param None

 * @retval None

 */

static void MX_GPIO_Init(void)

{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

 /* GPIO Ports Clock Enable */

 __HAL_RCC_GPIOB_CLK_ENABLE();

 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */

 HAL_GPIO_WritePin(GPIOD, LD4_Pin|LD3_Pin|LD5_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : CLK_IN_Pin */

 GPIO_InitStruct.Pin = CLK_IN_Pin;

 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

 GPIO_InitStruct.Pull = GPIO_NOPULL;

 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

 GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;

 HAL_GPIO_Init(CLK_IN_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : LD4_Pin LD3_Pin LD5_Pin */

 GPIO_InitStruct.Pin = LD4_Pin|LD3_Pin|LD5_Pin;

 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

 GPIO_InitStruct.Pull = GPIO_NOPULL;

 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;

 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pin : PD15 */

 GPIO_InitStruct.Pin = GPIO_PIN_15;

 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;

 GPIO_InitStruct.Pull = GPIO_NOPULL;

 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET);

 HAL_Delay(50);

   HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);

}

void Error_Handler(void)

{

}

#ifdef USE_FULL_ASSERT

/**

 * @brief Reports the name of the source file and the source line number

 *     where the assert_param error has occurred.

 * @param file: pointer to the source file name

 * @param line: assert_param error line source number

 * @retval None

 */

void assert_failed(uint8_t *file, uint32_t line)

{

 /* USER CODE BEGIN 6 */

 /* User can add his own implementation to report the file name and line number,

tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */

 /* USER CODE END 6 */

}

#endif /* USE_FULL_ASSERT */

/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KnarfB
Super User

When you read the adc_value bit by bit in the for loop, there is a pause after HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_SET); but no pause after HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13,GPIO_PIN_RESET);. Try adding a pause here too to meet min. low time.

Mbhir.1
Associate II

hey, did your hx711 work with this code ?