cancel
Showing results for 
Search instead for 
Did you mean: 

here do I find the .IOC file for STM32H7B3 JPEG_MJPEG_VideoDecodingFromOSPI example?

MGray.2
Associate

 I have not been able to generate a .ioc file using the CubeMX for the STEM32H7B3LI-DK board that has the correct values. I would like to know how, since selecting that board on a new STM32 project does not have the same values as the example without a .ioc file - the LTDC values are incorrect as well as the ospi - I would think selecting that STM32H7B31-DK would start off with the correct values for the peripherals, or I what am I doing wrong or misunderstand?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Projects without .IOC files were generally hand-crafted rather than machine generated, so more thought may have gone into them.

You'd want to check what clock, pin and peripheral settings were used in the project that worked.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..