2023-08-27 11:05 PM
Hello,
I work with STM32G484, with FDCAN. I want to create filter so only messages with my own CAN_ID will reach HAL_FDCAN_RxFifo0Callback.
I started by define the filter:
2023-08-28 12:35 AM
I'm unsure but I have HAL_FDCAN_Start and HAL_FDCAN_ActivateNotification with FDCAN_IT_RX_FIFO0_NEW_MESSAGE for active interrupt on every new message in HAL_FDCAN_RxFifo0Callback
and you also need to have HAL_FDCAN_ActivateNotification in FDCAN RX callback too.
2023-08-28 12:50 AM
I did all of this of course.
The problem is with the filter setting
Thank you
2023-08-28 1:48 AM
I had read your can config and your CAN id that I think that it's not oversize of Standard ID. I think it's an extended id.
so you should try to change IdType to extended one.
2023-08-28 2:31 AM
i work with CAN-ID of 10 to 200. So its not a problem of ID length. Any way I changed the ID type to extend and it still not working - passing all with regular filter only, and block all with the global filter
2024-02-27 2:24 AM
Hi prigo87!
Did you solve the issue? Mine is related:
H723 FDCAN1 and FDCAN2 - Page 2 - STMicroelectronics Community
Cheers!
2025-05-16 6:39 PM
I had this exact problem when trying to modify a project from extended IDs to standard IDs. In my case it turned out I had the FDCAN peripheral configured incorrectly in the .ioc file: it was set for 8 extended filter IDs and 0 standard filter IDs.
2025-08-07 6:42 PM
i has solved this issue as below
// 设置接收过滤器
FDCAN_FilterTypeDef sFilterConfig;
sFilterConfig.IdType = FDCAN_STANDARD_ID;
sFilterConfig.FilterIndex = 0;
sFilterConfig.FilterType = FDCAN_FILTER_MASK;
sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
sFilterConfig.FilterID1 = 0x002; // 设置过滤器ID1
sFilterConfig.FilterID2 = 0x7ff; // 设置过滤器ID2
if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
{
Error_Handler();
}
if(HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE) != HAL_OK)
{
Error_Handler();
}hfdcan1.Init.StdFiltersNbr = 1;you did not solve it, because you did not modify the stdFiltersNbr.
hope this will help you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.