2014-10-09 2:40 PM
Hello,
I'm very new to STM32, I recently switched from Microchip platform and I'm working on a Mac (which seems to make everything harder).I followed this very nice tutorialhttp://www.davidrojas.co.uk/stm32f3discovery-on-mac-os-x-using-eclipse-gcc-arm-and-openocd/
which got me up and running with the blink example with the STM32FDiscovery.Them I download the STM32CubeF3 and I'm trying to build the ''GPIO_IOToggle''example.There is no Eclipse example and neither I know how to import (or if its possible), them I started a blank project with my toolchain, which just gave me a blank main file.Them I add/replaced the .c and .h in the folders, when built I got a bunch of errors, because wrong paths I believe...After adding paths, this is my actual config:I've add#include
<stdint.h>#include
<stdio.h>To main.cNow I'm getting this weird error:/Users/valente/WorkSpace/STM32Resources/STM32Cube_FW_F3_V1.0.0/Drivers/STM32F3xx_HAL_Driver/Inc/stm32f3xx_hal_tim.h:1325:24: error: unknown type name 'TIM_TypeDef'
void TIM_OC3_SetConfig(TIM_TypeDef *TIMx, TIM_OC_InitTypeDef *OC_Config);But the files are all included...Any help is appreciated.Greetings.Renan2014-10-10 4:13 PM
Have you uncommented the #define HAL_TIM_MODULE_ENABLED section in
stm32f3xx_hal_conf.h?
2014-10-16 5:41 AM
No, I have not tried to comment this line. Actually I got really mad and deleted that project and I'm trying once again. I'll problably start another tread, now I believe I can better describe the problems
Thanks by your help! =D