Associate II
October 7, 2014
Question
Eclipse - IAR EWARM - Eclipse import project - java.lang.NullPointerException error
- October 7, 2014
- 3 replies
- 2254 views
Posted on October 07, 2014 at 22:30
I�m trying to import a STM32F401-Discovery Demo Project into the Eclipse IDE with errors.
stsw-stm32136 STM32F401-Discovery_FW_V1.0.0
I attached some pictures for reference only.
Some steps that I was following:
1.) I have instaled plug-ins into Eclipse Kepler from
http://eclipse-update.iar.com/
The plugin supports IAR Embedded Workbench for ARM (EWARM) 6.50.x/6.60.x/6.70.x/7.10.x.2.) After install and the reset I run again the Eclipse with and a plugin error.
''An error occurred while initializing the SDK IAR Toolchain for ARM - 6.x''3.) When I�m trying an import following: Import->IAR Embedded Workbench->Import IAR Embeded Workbench project
(see the attached pictures for ref.), another error happens:Failed to import project - An error occured during import:
java.lang.NullPointerException Refer to the error log for more details.I don�t know if evetually it is a problem from java due it was updated to Java Version 7 Update 67 or from IAR plugins or there are a problem on the project example: STM32F401-Discovery_FW_V1.0.0 I would like to say that I had already managed to import ok into another environment few months ago.
Have you the same problem? What is the miss on this procedure?
I�m sharing some information about this issue but Any help are welcome, please.Thanks in advance,
Greg/Brazil
===================================================== STM32F401C-DISCO - IAR Embedded Workbench 7.10.1.6735 - Eclipse Kepler 4.3.2 - Java 7 - 67 - Portugues/Brazilian language, Windows XP 32 bits - environment #stm32f401-discovery-eclipse-iar